Yokaichi Plant is a monumental plant that started operating in 1962 at Higashiomi-shi, Shiga Prefecture. It is one of the largest ceramics processing plants in the world. Processes from mixing and forming to firing take place at this plant. It is also known to be an environmentally friendly plant promoting a tree-planting project.
| Address | 4-1, Higashiokino 4-chome, Higashiomi-shi, Shiga 527-8558 Japan |
|---|---|
| Phone/Fax | 81-748-22-5500/81-748-23-1761 |

Take the JR Tokaido Line to Maibara Stn. or Ohmi-Hachiman Stn., change to the Ohmi Railway and detrain at Yokaichi Stn. From here it is 10 min. by Ohmi Bus to the Okuyama bus stop located in front of the office.