Global / MURATA MANUFACTURING CO., LTD.

Help

Murata Manufacturing Company, Ltd. Yasu Division

Overview

Yasu Plant is a relatively new plant which began its operation in 1987 at Yasu-shi, Shiga Prefecture. It conducts leading edge R&D for areas such as material development, development of production technology, semiconductors and thin-layer ultra-fine processing technology. Numerous research buildings and recreation facilities are located at its vast 250,000 m2 property. This plant also aims at reduction of greenhouse gas emission and industrial waste fluid by incorporating the cogeneration system as well as the latest industrial waste fluid reduction system.

Murata Manufacturing Company, Ltd. Yasu Plant

Page Top

Address/Phone

Address 2288, Oshinohara, Yasu-shi, Shiga 520-2393 Japan
Phone/Fax 81-77-587-5111/81-77-587-5205

Page Top

Map/Access

Map

Access

Access from the nearest station

20 min. by Ohmi Railway Bus from Yasu Stn. or Ohmi-Hachiman Stn. on the JR Biwako Line. Debus at the bus stop on the grounds of the office.

Home > About Murata > Network > Network - Japan > Murata Manufacturing Company, Ltd. Yasu Division

Help

Global / MURATA MANUFACTURING CO.,LTD.