From ultra technology at 100 millionth of a meter to RF technology in the region light, Murata's cutting-edge technology is always at the forefront of innovation.
Transparent ceramics were made possible through our challenge to achieve the ultimate nanoparticle-level downsizing of electronic components and nano-level grain boundary control, and now we are delving into the terahertz region pushing the limit of high frequency technology into the realm of optical light. Murata technology continuously evolves to achieve new characteristics, new functions and new values.
For example, pursuing miniaturization of monolithic ceramic capacitors will require minute ceramic materials with high crystallinity. This is where Murata's strength in being able to develop raw materials can be capitalized upon.
Check out Murata's brand-new, high-density ceramic particle materials that have been made possible through the optimization of manufacturing processes, ceramic/resin combination, etc.
Terahertz (THz) waves belong to a spectrum between radio waves and light waves. Murata will take up the challenge of finding related applications in unexplored fields of biotechnology, medicine and security.
Acousto-optics - detecting the wavelength of light through the interaction between surface acoustic waves and light waves - is one field in which Murata's original technology shines.
Cutting-Edge Technology